Hi: I have to make a new design, a PFC bucket converter.
In the new design ther is needed for ultra low power consumption, so I'll try if I can use a MSP430F51X2 and its high-resolution timer D.
But now I have some question as:
Can I set timer D0 or timer D1, to trigger ADC10_A, to start the an auto scan, in the Sequence-of-Channels mode.
Can I sette ADC10_A to trigger the DMA control, to move the result from ADC10_A, to a buffer i memory.
Keld