We have been using the TI MSPF5438 (non a) chip on several products for several years. Since most of our products are (relatively speaking) low volume, we have been using the on-chip bootstrap loader to install our software. Once we ironed out a few wrinkles, this has worked very well. We are using the IAR workbench, latest full version and are installing the hex file in TI.txt format via the bootstrap loader.
Recently we have moved to the MSPF5438(A) chip because TI says the non-A version should not be used for new projects. We took this to mean that TI probably will not produce or support the non-A version in the future. We have navigated the fairly modest changes necessary to change from non-a to a versions and all works well.
However, we have not been able to use the bootstrap loader to load software onto the A chip. I know from TI’s literature that the bootstrap loader on the A chip is modifiable whereas the non-A chip has a fixed bootstrap loader. So, the first question is whether the loader is even on the A chip and, if so, is it the same as the non-A? Are there differences that will have to be accommodated before we can use it to download a Hex file in the TI.txt format to the F5438A chip?
If the bootstrap loader is NOT already on the A chip, what is the procedure to install it, and should it then work as it did no the non-A chip? Has anyone had experience with this problem or have suggestions to help us find a solution for loading our software onto the MSPF5438A chip?