I messed up. I was on the road and made some changes to my code and programmed my part. I didn't back up the source code and have since made some more changes.
I need to test the changes, but also need to be able to go back to the version of code currently running (The version I didn't back up).
Is there anyway to upload the program out of a MSP430F2619 using Code Composer Studio Version: 5.3.0.00090, and MSP-FET430IF?
I've searched the menu, and help and can't find anything that tells me how to do this. Is it even possible?
Thanks