Other Parts Discussed in Thread: MSP430F5529
Hi
I have a custom board which receives power from 3 sources: JTAG, USB (VUSB) and PSU. The USB power line is fed to the VBUS pin of the CPU supplies the VUSB source. Each of these three sources are fed into BAT54C diodes to "select" the power source for the rest of the 3V circuit.
However, when I have JTAG and USB connected and add the PSU, the CPU gets fried somehow sometimes.
To note: I am working on a laptop that is unearthed, and after I blew the first board I also unearthed the external PSU that feeds my SMP PSU on the board. That worked for some time, but now a second board has blown as well and I don't know how to solve this issue.
The board has a MSP430F5529.
Perhaps someone knows how to help.