This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need to use a part of chip's FRAM memory to hold some variables. How can I specify it to compiler?
And what exactly happens when I write so:
const uint16_ foo;
I think that 'foo' will be in FRAM memory but, AFAIK, foo cannot be used in expression
foo = bar;
Thanks!
This declares a constant value. A storage location whose content will never change.It usually makes only sense for arrays of precalculated data or if you need to pass values by reference for some reason. Or if it is only kown that the value is constant, but not known, which value this will be (e.g. a serial number that is not known at compile-time).Iurii Vlasenko said:const uint16_ foo;
I think that 'foo' will be in FRAM memory
However, things declared as const go into non-volatile memory. They are not expected to ever change and cannot be changed by C code at all.
Since foo is a constant, it is read-only. The only case in which this would be allowed to pass through without an error (even though I doubt that any compiler will make this difference) is when bar is also a constant with the same value. Then the assignment is of course void.Iurii Vlasenko said:foo = bar;
If you want to put a variable (that can be written to) into FRAM, you can do so by preceding it with a pragma that tells the linker to put it into modifiable FRAM data section. See the compiler/linker manual for details.
Thank you very much!
Jens-Michael Gross said:a pragma that tells the linker to put it into modifiable FRAM data section. See the compiler/linker manual for details.
I've looked it up, but I liked another approach.
#define FRAM_VARS_START (uint16_t*)0x1800 uint16_t *ParsInFRAM; ParsInFRAM = CONF_VARS_START; ... *(ParsInFRAM++ ) = ParsWk[i]; ... ParsIn[i] = *(ParsInFRAM++);
The value of FRAM_VARS_START points to the Informatiom Memory of MSP430FR5726. It makes my code absolutely linked to the address, but it's OK for an array of configuration constants. And I can write to that location or read the constants in RAM (ParsIn[] or ParsWk[]). Now I try to organize a protection to this section - with a MPU of the MCU.
Of course this is a possible way to do it. It is, however, dangerous.Iurii Vlasenko said:I've looked it up, but I liked another approach.
It's better to just tell the linker through a pragma to place your data array into info memory. This way, you won't get a fixed address for it (well, it will likely be 0x1800 anyway), but the linker will take care for the allocation, so no conflicts can happen.
Thanks!
You explained all aspects of the question. "My mind is clear now"... (JC Superstar)
Still I think that limited and careful usage of "pointer" access (as I described earlier) may be accepted too. In small and simple projects, for example. Especially if I use information memory. Cannot imagin acidental double usage of it. Linker doesn't use it without special "pragmas", I think.
Besides, I'm not sure about the exact "pragma" way you say about :) Shall I use #pragma SET_DATA_SECTION? And, if I want the section to be located in a definite area (0x1800 infotmation memory), I have to tell Linker the 1-st address of that section. How?
Well, I have to grow up to it...
The linker has several sections defined in its control script. By default, the compiler adds linker information about putting code into TEXT section, variables into DATA section and so on. With the pragma, you tell the compiler to generate linker info for a different section then. Like the info memory sections which are defined (look into the linker command script for the exact names) but not normally used.Iurii Vlasenko said:Shall I use #pragma SET_DATA_SECTION? And, if I want the section to be located in a definite area (0x1800 infotmation memory), I have to tell Linker the 1-st address of that section. How?
As long as you are sure that this code is the only code that does it, it should work.Iurii Vlasenko said:Still I think that limited and careful usage of "pointer" access (as I described earlier) may be accepted too.
**Attention** This is a public forum