Hello!
Now I am wroking in a project which uses MSP430F5438A as main MCU,
I use MSP-FET430UIF to debug and download, it has no problem.
but when I try to use MSP-Gang to download, it occurred an error:
"ERROR 23: MCU device init failed"
so download routine failed.
We checked the circuit and found VCC power 3.3v is ok,
and 14pin JTAG connection is also ok refer to the MSP-Gang user guide.
I have ever tried use external power or supplied by programmer, but both method failed.
Now we can't find the problem,
Could you help to find the reason for it?
Thank you.