This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How do I setup the IAR Debug Output

I am picking up a project from an engineer that is no longer with the company. I had to create a new project. I believe I have everything setup, but for the Output it has a .d43 file instead of the text file that was in the other project. I need the .txt file so I can download the results into the MSP430. How do I change the output.

Or can I use the .d43 file directly with the MSP-GANG?

**Attention** This is a public forum