This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EXPCC430RF4 board not detected

Hello,

we are working on the EXPCC430RF4 board and having it detected on windows 7 and windows XP has proven a challenge.

Problem

When we launch the GUI for the network topology, the base board is not recognized, the GUI doesn't display data from it and the network is not represented.

Tools

  • Windows XP SP3 and Windows 7
  • CCSv5.5
  • user experience package at http://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/MSP430EXPCC430RFUE/latest/index_FDS.html

What we tried

following the instructions on the users manual at http://www.ti.com/lit/ug/slau460/slau460.pdf we did:

  • fresh install of windows 7, then installed CCSv5 with MSP430 support, and the user experience package (GUI + driver installer)
  • fresh install of windows XP then CCSv5 with MSP430 support and user experience package
In each case we tried to install CCS first then the user experience package, or only the package.
We also tried to run the USB driver installer alone without CCS installed.
We also tried to right-click on the .inf file next to the executable.
In the device manager, under "Other devices" we see an "Unknown device" which might not be related but which comes back if we deinstall it and run the USB driver installer again. This device has Hardware Ids: "ACPI\VPC2004" and "*VPC2004".
When we plug-in the main board, it is powered up, and the network seems to be working just fine. The satellite pairs with the main board.
Any suggestion on this issue would be greatly appreciated.
Thanks,
Jacques

**Attention** This is a public forum