I have made two board which communicate with each other. One is master & other is slave. I have FT232 for that. Problem is slave board is powered via usb on which FT232 is connected & if its is connected & master is off. Even then TXD & RXD pin of uart of master has some 3.3V. Will it destroy the master.
How to avoid it.