Other Parts Discussed in Thread: MSP430F5528
Hi,
I'm having trouble with a MSP430F5528 system which is powered from USB. Hardware and software design are almost finished. During testing I noticed that in rare cases the CPU does not start software execution after plugging in the USB cable. In these cases the PC immediately detects presence of the USB device which should not happen because the USB module is not enabled yet. I cannot trace the problem by debugging because it only occurs without debugger. I think it is a hardware problem. It depends on the way I plug in the USB cable (wedged or even, slowly or quickly) and it only occurs with the type A plug side. I have already replaced the cable. Could there be a latch-up problem if DP or DM are connected before +5V or GND?
The CPU is not powered from VUSB but from an external 3.3V LDO.
Here is the relevant section of my circuit:
Can anyone help me please?
Regards Jan