Hello,
I am looking to implement a 4V solar charged LiFePO4 to drive a 350mA portable LED light. I would like to implement it with the MPS430, the BQ24650, and a BQ24710 gauge, all to the appropriate driver for the LED. Looking at app note SLAA529A by Tyler Witt, which is similar but for a LiPoly battery: Is this possible to do with the 24650 solar charger instead of the 24230?? The set up for CE is different. I would also like if possible to have the 24710 gauge be programmed for either a NiMH or LiFePO4 during production. What do you suggest?
Thanks!