Other Parts Discussed in Thread: MSP430G2452, MSP-TS430PW28A
Hi there,
I use a MSP430G2452 with the eval board MSP-TS430PW28A.
I would like to use XT1 with 32kHz. When I use the debugger, it dosen't work properly and it stays in oscillator fault condition. If I disconnect the debugger, it works.
I would like to know why it doesn't work with the debugger...
I use this code, it is writen by TI:
//******************************************************************************
// MSP430G2xx2 Demo - LFXT1 Oscillator Fault Detection
//
// Description: System runs normally in LPM3 with WDT timer clocked by
// 32kHz ACLK with a 1x4 second interrupt. P1.0 is normally pulsed every
// second inside WDT interrupt. If an LFXT1 oscillator fault occurs,
// NMI is requested forcing exit from LPM3. P1.0 is toggled rapidly by software
// as long as LFXT1 oscillator fault is present. Assumed only LFXT1 as NMI
// source - code does not check for other NMI sources.
// ACLK = LFXT1 = 32768, MCLK = SMCLK = Default DCO
//
// //*External watch crystal on XIN XOUT is required for ACLK*//
//
//
// MSP430G2xx2
// ---------------
// /|\| XIN|-
// | | | 32kHz
// --|RST XOUT|-
// | |
// | P1.0|-->LED
//
// D. Dang
// Texas Instruments Inc.
// December 2010
// Built with CCS Version 4.2.0 and IAR Embedded Workbench Version: 5.10
//******************************************************************************
#include <msp430.h>
volatile unsigned int i;
int main(void)
{
WDTCTL = WDT_ADLY_1000; // WDT 1s interval timer
IE1 |= WDTIE; // Enable WDT interrupt
P1DIR = 0xFF; // All P1.x outputs
P1OUT = 0; // All P1.x reset
P2DIR = 0xFF; // All P2.x outputs
P2OUT = 0; // All P2.x reset
// An immedate Osc Fault will occur next
IE1 |= OFIE; // Enable Osc Fault
while(1)
{
P1OUT ^= 0x01; // Toggle P1.0 using exclusive-OR
_BIS_SR(LPM3_bits + GIE); // Enter LPM3 w/interrupt
}
}
#pragma vector=WDT_VECTOR
__interrupt void watchdog_timer (void)
{
_BIC_SR_IRQ(LPM3_bits); // Clear LPM3 bits from 0(SR)
}
#pragma vector=NMI_VECTOR
__interrupt void nmi_ (void)
{
do
{
IFG1 &= ~OFIFG; // Clear OSCFault flag
for (i = 0xFFF; i > 0; i--); // Time for flag to set
P1OUT ^= 0x01; // Toggle P1.0 using exclusive-OR
}
while (IFG1 & OFIFG); // OSCFault flag still set?
IE1 |= OFIE; // Enable Osc Fault
}
Thank you in advance