Other Parts Discussed in Thread: MSP430F5529
Hello everyone, I am trying to figure out how to use the Touch Pads on the MSP430F5529 micro-controller to get the user to set time, The problem Statement is as Follows:
When the program starts, it will start displaying time starting from 00:00:00.
Pressing touch sensitive PAD4 causes the program to enter time adjustment mode, and while in time adjustment mode:
- Seconds will be immediately set to zero
- Touching PAD1 increases the hours (from 0 to 23, and then back to zero again)
- Touching PAD2 increases the minutes (from 0 to 59, and then back to 0 again)
- Touching PAD4 again will cause the program to run normally, displaying the current time that was entered by the user.
/******************************************************************************* * * UserExperience.c - Main Application * * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/ * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ******************************************************************************/ /******************************************************************************* * Modified by: Kevin Moore, NAIT * Date: Nov.26, 2013 * * This program demonstrates the use of the capacitive * touch pad library. * * Students may use this project and its source code * to complete lab work in ELTRO1102 (Embedded 1). * * Note that the library Touchpad.c and its header file * have many dependencies. These additional files are * incorporated into this demonstration project. * * * *******************************************************************************/ /******************************************************************************** * Include Directives ********************************************************************************/ #include <stdint.h> #include "msp430.h" #include <HAL_PMM.h> #include "HAL_UCS.h" #include "HAL_Board.h" #include "HAL_Dogs102x6.h" #include <HAL_Dogs102x6_B.h> #include "structure.h" #include "CTS_Layer.h" #include <TouchPad.h> #include <intrinsics.h> //contains declaration for _delay_cycles() #define CHAR_WIDTH 6 /******************************************************************************** * Function Declarations * See definitions below function main for more information * if you are interested. ********************************************************************************/ void Start(void); void StartLCD(void); void StartTouchPads(void); void DisplayTime(int nSec, int nMin, int nHours); void main(void) {//start main function volatile unsigned int nTouchPad = 0; Start(); //initialize hardware int nMode1=1; while(1) {//start first while loop nTouchPad = GetTouchPads(); //detect which pad is touched //set a break point on this line //touch a pad, and observe what happens //to the variable nTouchPad if (nMode1 ==1) {//if loop start int nSS = 0, nMM = 0, nHH = 0; Start(); //init hardware while(1) {//while loop 1 start Dogs102x6_clearRow(0); DisplayTime(nSS, nMM, nHH); nSS++; if (nSS > 59) { nMM = nMM + 1; nSS=0; } if (nMM > 59) { nHH = nHH + 1; nMM = 0; } if (nHH > 23) { nHH = 0; nMM = 0; nSS = 0; } _delay_cycles (1048576-500); /*This part of the program will enable user to set time using the touch pads*/ if (nTouchPad==4) {nMode1=2; }//while loop 1 ends //This part of the program will define what happens when the nMode is equal to 2 if(nMode1==2) {//if nMode 2 Starts nTouchPad = GetTouchPads(); nSS = 0; if(nTouchPad ==1) { nHH++; __delay_cycles(27000000); } if(nTouchPad ==2) { nMM++; __delay_cycles(27000000); }if(nTouchPad ==4) { nMode1=1; __delay_cycles(27000000); } } //if nMode 2 ends }//while loop end }//end first while loop }//main function end } /* *********************************************************************** * Function: Start * Parameters: None * Returns nothing. Initializes all hardware for this demo program, * involving the LCD and touch pads. * * ***********************************************************************/ void Start(void) { WDTCTL = WDTPW + WDTHOLD; //disable watchdog timer Board_init(); //initialize MSP430 pins //Buttons_init(BUTTON_ALL); Dogs102x6_init(); Dogs102x6_backlightInit(); Dogs102x6_setBacklight(3); Dogs102x6_setContrast(7); Dogs102x6_clearScreen(); } /* *********************************************************************** * Function: Start * Parameters: None * Returns nothing. Initializes all hardware for this demo program, * involving the LCD and touch pads. * * ***********************************************************************/ void StartLCD(void) { Dogs102x6_init(); //init LCD Dogs102x6_backlightInit(); //turn on back light Dogs102x6_setBacklight(11); //set back light intensity Dogs102x6_setContrast(11); //set LCD pixel contrast Dogs102x6_clearScreen(); //clear the LCD } void StartTouchPads(void) { // Set Vcore to accomodate for max. allowed system speed SetVCore(3); // Use 32.768kHz XTAL as reference LFXT_Start(XT1DRIVE_0); // Set system clock to max (25MHz) Init_FLL_Settle(25000, 762); TI_CAPT_Init_Baseline(&slider); //measure baseline capacitance //must be called while no pads are touched } void DisplayTime(int nSec, int nMin, int nHours) { Dogs102x6_intDrawXY(0,0, nHours,DOGS102x6_DRAW_NORMAL); Dogs102x6_stringDrawXY(CHAR_WIDTH*2+1, 0, ":", 0); Dogs102x6_intDrawXY(0,CHAR_WIDTH*3+1, nMin, DOGS102x6_DRAW_NORMAL); Dogs102x6_stringDrawXY(CHAR_WIDTH*5+1, 0, ":", 0); Dogs102x6_intDrawXY(0,CHAR_WIDTH*6+1, nSec,DOGS102x6_DRAW_NORMAL); }Above is My code and I am not sure why I am not being able to get the Touch Pads to alter my time in any way! Any Help is greatly appreciated.