All,
Thank you so much for reading and responding to this post. I reallly appreciate it.
1.) We are using the MSP430F5528 and want to run as fast as possible. That being said, what crystal frequency should we be using for XT2?
2.) The maximum processor frequency accorindg to the datasheet looks to be 25 MHz.
3.) When I look at the specifications in the datasheet for XT2 I see:
Mode 0 - frequency range 4-8 MHz
Mode 1 - frequency range 8-16 MHz
Mode 2 - frequency range 16-24 MHz
Mode 3 - frequency range 24-32 MHz
Isn't mode 3 invalid since the maximum processor frequecy 25 Mhz not 32 MHz?
Please advise.
Thanks.