Other Parts Discussed in Thread: CC1101, SIMPLICITI, MSP430F5529
Hi,
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC1101, SIMPLICITI, MSP430F5529
Hi,
No, this one is about the DMA9 erratum which is related to the eUSCI module. You don't have an eUSCI module.RAHUL TT said:A somewhat similar issue was noticed here
However, it might be your DMA code that has some racing condition. DMA is edge triggered. When you reconfigure DMA for the next data block or something like that, and an RX event happens before the DMA is armed again, then it will miss this trigger. And since no DMA happens to read RXBUF and clear RXIFG, no more RX triggers will come.
Hi,
Thank you very much for your response. As you said, it seems like the DMA RX code has racing condition. The RXIFG flag remains set after the DMA hangs. I think this racing condition does not occur in our DMA UART TX code since data transfer occurs only after the completion of previous transfer.
But in case of DMA UART RX, bytes are received continuously from the application at a high rate. When the Wireless data rate is high, RF receive ISR and entering critical sections will be more which leads to a delay in handling DMA ISR where we are reconfiguring the DMA for the next data block.
Please let me know by what changes should I make to avoid this racing condition?
Thanks
Rahul
You could run the DMA in repeated mode. So the interrupt will tell you that the buffer was full, but DMA will seamlessly continue to fill the buffer from start with new incoming data.
Of course this may rise other problems, but at least you won't have the DMA stopped whiel data arrives, and then stalled.
Another possible way would be to check whether RXIFG is set when you have just readied the DMA. If it is, then the DMA has missed a byte, and you can manually clear and re-set the RXIFG flag, to trigger the DMA and get it back into the gear.
Hi,
Thank you for your response.
Jens-Michael Gross said:Another possible way would be to check whether RXIFG is set when you have just readied the DMA. If it is, then the DMA has missed a byte, and you can manually clear and re-set the RXIFG flag, to trigger the DMA and get it back into the gear.
Since we cannot confirm that only 1 byte is missed by DMA and every byte is critical in our application. We prefer to go with the 1st option.
Jens-Michael Gross said:You could run the DMA in repeated mode. So the interrupt will tell you that the buffer was full, but DMA will seamlessly continue to fill the buffer from start with new incoming data.
Thanks
**Attention** This is a public forum