This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

three phase energy meter



Hello,

I need to monitor 3 phase voltage in my application. I looked at some of the devices which are recommended for 3 phase energy metering like MSP430F67791 and MSP430F471xx or AFEs. Applications notes of these devices talk about only Star connection of the 3 phase input and load with Neutral. I am looking at the scenario of Delta connection or Star connection without Neutral. Can these devices work in that scenario. If not can somebody suggest the right devices.

Thanks.

Vijayeendra

**Attention** This is a public forum