Hi,
I am currently working on the GSM / GPRS interfacing with the MSP430F5435 module. I have interfaced the system that can send the data from MSP430F5435 flash to the server based on TCP/ IP protocol. The reception at the server is very slow. I mean the data is received almost after 15 minutes. How do I resolve this issue?
Also, I am trying to get the data from server to device and the protocol being used is TCP/ IP. How do I track the dynamic IP address of the SIM card that is being used ? What are the AT commands and functions to be used while programming?
Thank you.