This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F2272 flash routines

I have to write 300 Byte of data in flash.

I write this simple routine, but i think that there is ana error because this routine stops my f2272.

can anyone please help me?

thank'you very much.

This is the function:

 

 

 

 

 

 

void

 

write_FlashByte(char value, uint8 index)

{

volatile

 

char

CAL_DATA[FLASH_MEM_DIM];

char

 

 *Flash_ptr; // Flash pointer

uint16 i;

FCTL2 = FWKEY + FSSEL0 + FN1;

 

// MCLK/3 for Flash Timing Generator

Flash_ptr =0x0fe00

; // Initialize Flash pointer

 

 

 

for (i = 0; i < FLASH_MEM_DIM; i++) //save old data in memory

{

CAL_DATA[i] = *Flash_ptr++;

}

Flash_ptr = (

char*)0x0fe00;// 0xfd00 ; // Initialize Flash pointer

FCTL3 = FWKEY;

// Clear Lock bit

FCTL1 = FWKEY + ERASE + EEI;

// Set Erase bit, allow interrupts

*Flash_ptr = 0;

// Dummy write to erase Flash seg

FCTL1 = FWKEY + WRT;

// Set WRT bit for write operation

/************************************************************

at this point the f2272 remains blocked

*************************************************************/

 

for (i = 0; i < ADDR_DATA_MEM; i++) //save old data in memory

{

 

if(i == index)

*Flash_ptr++ = value;

//write new value to flash

 

else

*Flash_ptr++ = CAL_DATA[i];

// Write old value to flash

}

FCTL1 = FWKEY;

// Clear WRT bit

FCTL3 = FWKEY + LOCK;

// Set LOCK bit

}

 

 

 

Help me please!

thank'you!

**Attention** This is a public forum