Other Parts Discussed in Thread: MSP430F2619
I am looking at the DMACTL0 description in SLAU144, and am disappointed to see that UCB1TXIFG and UCB1RXIFG are not on the list of selectable triggers. Am I missing something? Is there any way to trigger on those flags anyway?
The best solution I can think of at this point is triggering off of UCA1 and having UCA1 mirror everything UCB1 does using a "creative" block transfer that writes the appropriate configuration for both interfaces at the same time. This is ugly with possible unpredicatable behavior (not to mention it couldn't be any less portable) and I really don't want to do it, so I would definitely appreciate a better suggestion.
I know I could use interrupts, but I am pretty much continuously sampling an ADC and already have other timing-sensitive interrupts, so I am trying hard to avoid having more interrupts fire off all over the place.
I am using an MSP430F2619. Ideally, I would be able to just rev the board to pick whatever USCI I want, but alas, that is not possible right now, so I have to use UCB1.
Edit: The above "solution" I was thinking of takes 20 clock cycles per transcieved byte in my application when an interrupt only takes 14, so it's not any use. If no one has any better ideas, I'll just do what I need to do in the main thread and have other stuff wait...