This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART tutorial for beginners

Hello,

I am using the EZ430-RF2500 Development kit and I am trying to learn how to communicate from the chip to the computer. From what I deciphered, it is easiest to do this by using the UART method. However, I am running into a few bugs. I am running the standard "Hello World" tutorial code, but I am not getting any stimuli on my program. Do I need to download additional software to complete this process? I am currently using the IAR kickstarter software to program/debug my board. My future goal is to create a file and write/write-over data to it. Is this possible? I've tried looking for online tutorials for this situation but to this day I couldn't find any. If you know of some please let me know! Lastly, my code for the "Hello World" simulation is below.

#include  "msp430x22x4.h"

const char string1[] = { "Hello World\r\n" };
  unsigned int i;

void main(void)
{
  WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
  P1DIR = 0xFF;                             // All P1.x outputs
  P1OUT = 0;                                // All P1.x reset
  P2DIR = 0xFF;                             // All P2.x outputs
  P2OUT = 0;                                // All P2.x reset
  P3SEL = 0x30;                             // P3.4,5 = USCI_A0 TXD/RXD
  P3DIR = 0xFF;                             // All P3.x outputs
  P3OUT = 0;                                // All P3.x reset
  P4DIR = 0xFF;                             // All P4.x outputs
  P4OUT = 0;                                // All P4.x reset
  UCA0CTL1 |= UCSSEL_1;                     // CLK = ACLK
  UCA0BR0 = 0x03;                           // 32kHz/9600 = 3.41
  UCA0BR1 = 0x00;                           //
  UCA0MCTL = UCBRS1 + UCBRS0;               // Modulation UCBRSx = 3
  UCA0CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**
  IE2 |= UCA0RXIE;                          // Enable USCI_A0 RX interrupt

  __bis_SR_register(LPM3_bits + GIE);       // Enter LPM3 w/ int until Byte RXed
}

#pragma vector=USCIAB0TX_VECTOR
__interrupt void USCI0TX_ISR(void)
{
  UCA0TXBUF = string1[i++];                 // TX next character

  if (i == sizeof string1 - 1)              // TX over?
    IE2 &= ~UCA0TXIE;                       // Disable USCI_A0 TX interrupt
}

#pragma vector=USCIAB0RX_VECTOR
__interrupt void USCI0RX_ISR(void)
{
  if (UCA0RXBUF == 'u')                     // 'u' received?
  {
    i = 0;
    IE2 |= UCA0TXIE;                        // Enable USCI_A0 TX interrupt
    UCA0TXBUF = string1[i++];
  }
}

**Attention** This is a public forum