This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMMSWBOR triggered itself

Hi all,

i have run some long term test on one of my product. It goes several time at cold temperature of -40°C and I can observe some reboots, especially during these cold step. My logs tell that all reboot are due to PMMSWBOR. Indeed, I send the SYSRSTIV value and it returns always 0x07 or 0x06. (by the way, how LSB could be set?).

If I understand, PMMSWBOR means that the the reboot is software initiated? However I have nothing in the code doing this. So what could be the other source of a PMMSWBOR?

FYI, this product is running on battery and the MSP is supplied with the lower voltage (1.8V). So I thought that the reboot could come from a voltage dropping below cutoff voltage. But I should have a SVSPOR (Supply Voltage Supervisor)?

Do you have any information/advise about that?

Thanks a lot,

Sébastien

**Attention** This is a public forum