This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Grace Problem

Hi,

I cannot use grace and I cannot understand why. Trying for about 5 hours and going insane.

I don't have any problem with normal coding-compiling etc. However, when I try to use grace it gives these warnings:

See details below... 
  Warning: Configuration 'Debug' - build-option setting '-I${COM_TI_MCU_MSP430WARE_INSTALL_DIR}' is not recognized. Ignoring...
  Warning: Configuration 'Debug' - build-option setting '-I${COM_TI_MCU_MSP430WARE_INSTALL_DIR}/driverlib' is not recognized. Ignoring...
  Warning: Configuration 'Release' - build-option setting '-I${COM_TI_MCU_MSP430WARE_INSTALL_DIR}' is not recognized. Ignoring...
  Warning: Configuration 'Release' - build-option setting '-I${COM_TI_MCU_MSP430WARE_INSTALL_DIR}/driverlib' is not recognized. Ignoring...

then, when I say "Build", it says : #1965 cannot open source file "ti/mcu/msp430/Grace.h"

I thought that this is a path problem, but I cannot find these directories in my computer.

When I search on the internet, the only result says that this is because Turkish Windows.

AFAIK, grace is coming with CCS, I didn't make any extra installations.

I am using CCS Version: 5.5.0.00077, Grace 2.20.1.12, Win7 32Bit, MSP430 Launchpad with 430G2553

Any other necessary details?

What causes this problem? If it is Tr Windows, what is the solution? I don't want to change my OS.

Thanks is advance.

**Attention** This is a public forum