Hi,
I am planning to use a sampling rate of 100Hz meaning that each sample will be collected in 10ms using the timer and by suing the 32KHz ACLK.can someone explain what should be the minimum and maximum time needed for the ADC12 sample conversion.
what factors will effect the ADC12 conversion time calculation and how the selected(min and max) time will effect the conversion result.
thankyou.