Other Parts Discussed in Thread: MSP-TS430PW28A, MSP430G2553
So for a class I have to design a circuit board where the MSP430G2553 will be surface mounted. I have the MSP-FET430U28A programming kit. The problem is that I need to be able to program the MSP430G2553 while it is on the circuit board that I am designing. In summary I need to recreate the circuit from the 14 pin serial on the development board to the actual chip. I have found the actual schematic for the development board MSP-TS430PW28A, I am not 100% sure on which connections I need to make. I will have a separate power supply so no power will be needed from the development board. From what I gather I need to connect pins 1,3,5,7 on the 14 pin serial cord to pins 1.7,1.6,1.5,1.4 respectively. Any help is much appreciated...
For refrence http://www.ti.com/tool/msp-ts430pw28a.. and download the technical documents the schematic is located in there...
Thanks
Kelen