This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

*** Serial port and E-meter

I measured the serial port pins' voltage on the energy meter when it is not connected to the computer which is given by the following link.

http://www.ti.com/tool/TIDM-THREEPHASEMETER

I got nothing! 0!   

Should I supposed to get voltage on pins number 2 and 3 which are TX and TR? Maybe the voltage is too low to see on the multi-meter?

What do you think?

**Attention** This is a public forum