This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

eZ430-RF2500T with MSP430F5438 Dev. Kit

Other Parts Discussed in Thread: MSP430F5438

Hello,


I am using eZ430-RF2500T with MSP430F5438 Development Board.

 

I want to do the following:

I intend to use three modules of eZ430-RF2500T. In this, two eZ430-RF2500T will act as a End Devices and one will act as an Access Point.

The Access Point will be attached to the MSP430F5438 Dev Kit. The data sent by the End Devices will be received by the Access Point.

The data received and Access Point's own data will be displayed on the TFT Display of MSP430F5438  Dev Kit.

 

In order to achieve the above, I will have to program eZ430-RF2500T module and MSP430F5438 seperately.

How can I set the communication between eZ430-RF2500T and MSP430F5438?

Will I have to use SPI port available on the extension connector of eZ430-RF2550T?

The SPI port available on eZ430-RF2500T & MSP430F5438 are both host..... So how can I communicate??

Has anyone used eZ430-RF2500T and MSP430F5438 dev. kit together for RF Networking????


Regards

Sushil Raut

**Attention** This is a public forum