Hi,
where can I get more information about LCD segment mapping used in EVM430-F6779? Where can I buy it?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
where can I get more information about LCD segment mapping used in EVM430-F6779? Where can I buy it?
Thanks.
Rafael Ramos said:where can I get more information about LCD segment mapping used in EVM430-F6779?
Download the zip file that goes along with the EVM kit. The link is on the product page of the kit. In the source file LCD-internal.c it says that the LCD is a T218010. (Strange that the zip file doesn't contain a bill-of-materials document, schematic is in the PDF app note).
Rafael Ramos said:Where can I buy it?
The EVM? Or the LCD? Buy the EVM right from the product page for the EVM. You can google the LCD part number to try to find technical data and a source.
Brian Boorman said:Download the zip file that goes along with the EVM kit. The link is on the product page of the kit. In the source file LCD-internal.c it says that the LCD is a T218010. (Strange that the zip file doesn't contain a bill-of-materials document, schematic is in the PDF app note).
It seems that EVM430-F6779 uses a different display. All segments (from S0 to S39) are mapped to LCD.
Brian Boorman said:The EVM? Or the LCD? Buy the EVM right from the product page for the EVM. You can google the LCD part number to try to find technical data and a source.
**Attention** This is a public forum