This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SMCLK pin MSP430F5510 LQFP48

Other Parts Discussed in Thread: MSP430F5510

Hello,

I'm using a MSP430F5510 with the LQFP48 package. In my application I use also a 8th Order Lowpass filter. the frequency corner is choose with an input clock. Today somebody tell me that we need to choose the frequency corner of the filter with the microcontroller so I though about using the SMCLK pin of the MSP430 with a divider. But with the 48pin package there is no SMCLK pin. I Prefer use the 48LQFP package because all te pcb is done and this package is easyest to solder.

My application need only an SPI, a serial port and some input/ouput pin. Is there another MSP430 with the LQFP48 package and the SMCLK pin ?

Thanks

Laurent

**Attention** This is a public forum