This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Getting undefined reference in custom class



I'm attempting to utilize an open-source project called UTFT-Energia.

Unfortunately, when I attempt to test out the code, I receive the following errors:

/UTFT_Bitmap_Launchpad.cpp:34: undefined reference to `UTFT::InitLCD(unsigned char)'

/UTFT_Bitmap_Launchpad.cpp:36: undefined reference to `SmallFont'

/UTFT_Bitmap_Launchpad.cpp:36: undefined reference to `UTFT::setFont(unsigned char*)'

The UTFT class is defined in the header file.

Any help getting this annoying error message to disappear would be appreciated. Thanks in advance!

The header file is UTFT.h:

#ifndef UTFT_h
#define UTFT_h

#define UTFT_VERSION  241

#define LEFT 0
#define RIGHT 9999
#define CENTER 9998

#define PORTRAIT 0
#define LANDSCAPE 1

#define HX8347A			0
#define ILI9327			1
#define SSD1289			2
#define ILI9325C		3
#define ILI9325D_8		4
#define ILI9325D_16		5
#define HX8340B_8		6
#define HX8340B_S		7
#define HX8352A			8
#define ST7735			9
#define PCF8833			10
#define S1D19122		11
#define SSD1963_480		12
#define SSD1963_800		13
#define S6D1121_8		14
#define S6D1121_16		15
#define	SSD1289LATCHED	16
#define ILI9320_8		17
#define ILI9320_16		18
#define SSD1289_8		19
#define SSD1963_800ALT		20
#define ILI9481			21

#define ITDB32			0	// HX8347-A (16bit)
#define ITDB32WC		1	// ILI9327  (16bit)
#define TFT01_32W		1	// ILI9327	(16bit)
#define ITDB32S			2	// SSD1289  (16bit)
#define TFT01_32		2	// SSD1289  (16bit)
#define CTE32			2	// SSD1289  (16bit)
#define GEEE32			2	// SSD1289  (16bit)
#define ITDB24			3	// ILI9325C (8bit)
#define ITDB24D			4	// ILI9325D (8bit)
#define ITDB24DWOT		4	// ILI9325D (8bit)
#define ITDB28			4	// ILI9325D (8bit)
#define TFT01_24_8		4	// ILI9325D (8bit)
#define TFT01_24_16		5	// ILI9325D (16bit)
#define ITDB22			6	// HX8340-B (8bit)
#define GEEE22			6	// HX8340-B (8bit)
#define ITDB22SP		7	// HX8340-B (Serial)
#define ITDB32WD		8	// HX8352-A (16bit)
#define TFT01_32WD		8	// HX8352-A	(16bit)
#define ITDB18SP		9	// ST7735   (Serial)
#define LPH9135			10	// PCF8833	(Serial)
#define ITDB25H			11	// S1D19122	(16bit)
#define ITDB43			12	// SSD1963	(16bit) 480x272
#define ITDB50			13	// SSD1963	(16bit) 800x480
#define TFT01_50		13	// SSD1963      (16bit) 800x480
#define CTE50			13	// SSD1963      (16bit) 800x480
#define ITDB24E_8		14	// S6D1121	(8bit)
#define ITDB24E_16		15	// S6D1121	(16bit)
#define INFINIT32		16	// SSD1289	(Latched 16bit) -- Legacy, will be removed later
#define ELEE32_REVA		16	// SSD1289	(Latched 16bit)
#define GEEE24			17	// ILI9320	(8bit)
#define GEEE28			18	// ILI9320	(16bit)
#define ELEE32_REVB		19	// SSD1289	(8bit)
#define TFT01_70		20	// SSD1963      (16bit) 800x480 Alternative Init
#define CTE70			20	// SSD1963      (16bit) 800x480 Alternative Init
#define CTE32HR			21	// ILI9481      (16bit)

#define SERIAL_4PIN		4
#define SERIAL_5PIN		5
#define LATCHED_16		17

//*********************************
// COLORS
//*********************************
// VGA color palette
#define VGA_BLACK		0x0000
#define VGA_WHITE		0xFFFF
#define VGA_RED			0xF800
#define VGA_GREEN		0x0400
#define VGA_BLUE		0x001F
#define VGA_SILVER		0xC618
#define VGA_GRAY		0x8410
#define VGA_MAROON		0x8000
#define VGA_YELLOW		0xFFE0
#define VGA_OLIVE		0x8400
#define VGA_LIME		0x07E0
#define VGA_AQUA		0x07FF
#define VGA_TEAL		0x0410
#define VGA_NAVY		0x0010
#define VGA_FUCHSIA		0xF81F
#define VGA_PURPLE		0x8010
#define VGA_TRANSPARENT		0xFFFFFFFF

#if defined(ENERGIA)
	#include "Energia.h"
	#if defined(__LM4F120H5QR__)
		#include "hardware/lm4f/HW_LM4F_defines.h"
	#elif defined(__MSP430__)
		#include "HW_MSP430_defines.h"
	#else
		#error "unknown Energia target"
	#endif
#elif defined(ARDUINO)
	#if defined(__AVR__)
		#include "Arduino.h"
		#include "hardware/avr/HW_AVR_defines.h"
	#elif defined(__arm__)
		#include "Arduino.h"
		#include "hardware/arm/HW_ARM_defines.h"
	#elif defined(__PIC32MX__)
		#include "WProgram.h"
		#include "hardware/pic32/HW_PIC32_defines.h"
	#else
		#error "unknown Arduino target"
	#endif
#endif

struct _current_font
{
	uint8_t* font;
	uint8_t x_size;
	uint8_t y_size;
	uint8_t offset;
	uint8_t numchars;
};

class UTFT
{
	public:
		UTFT();
		UTFT(byte model, int RS, int WR,int CS, int RST, int SER=0);
		void InitLCD(byte orientation=LANDSCAPE);
		void clrScr();
		void drawPixel(int x, int y);
		void drawLine(int x1, int y1, int x2, int y2);
		void fillScr(byte r, byte g, byte b);
		void fillScr(word color);
		void drawRect(int x1, int y1, int x2, int y2);
		void drawRoundRect(int x1, int y1, int x2, int y2);
		void fillRect(int x1, int y1, int x2, int y2);
		void fillRoundRect(int x1, int y1, int x2, int y2);
		void drawCircle(int x, int y, int radius);
		void fillCircle(int x, int y, int radius);
		void setColor(byte r, byte g, byte b);
		void setColor(word color);
		word getColor();
		void setBackColor(byte r, byte g, byte b);
		void setBackColor(uint32_t color);
		word getBackColor();
		void print(char *st, int x, int y, int deg=0);
		void print(String st, int x, int y, int deg=0);
		void printNumI(long num, int x, int y, int length=0, char filler=' ');
		void printNumF(double num, byte dec, int x, int y, char divider='.', int length=0, char filler=' ');
		void setFont(uint8_t* font);
		uint8_t* getFont();
		uint8_t getFontXsize();
		uint8_t getFontYsize();
		void drawBitmap(int x, int y, int sx, int sy, bitmapdatatype data, int scale=1);
		void drawBitmap(int x, int y, int sx, int sy, bitmapdatatype data, int deg, int rox, int roy);
		void lcdOff();
		void lcdOn();
		void setContrast(char c);
		int  getDisplayXSize();
		int	 getDisplayYSize();

/*
      The functions and variables below should not normally be used.
      They have been left publicly available for use in add-on libraries
      that might need access to the lower level functions of UTFT.

      Please note that these functions and variables are not documented
      and I do not provide support on how to use them.
*/
		byte fch, fcl, bch, bcl;
		byte orient;
		long disp_x_size, disp_y_size;
		byte display_model, display_transfer_mode, display_serial_mode;
		regtype P_RS, P_WR, P_CS, P_RST, P_SDA, P_SCL, P_ALE;
		regsize B_RS, B_WR, B_CS, B_RST, B_SDA, B_SCL, B_ALE;
		byte RS, WR, CS, RST, SER;
		_current_font	cfont;
		boolean _transparent;

		void initPins();
		void LCD_Writ_Bus(char VH,char VL, byte mode);
		void LCD_Write_COM(char VL);
		void LCD_Write_DATA(char VH,char VL);
		void LCD_Write_DATA(char VL);
		void LCD_Write_COM_DATA(char com1,int dat1);
		void _hw_special_init();
		void setPixel(word color);
		void drawHLine(int x, int y, int l);
		void drawVLine(int x, int y, int l);
		void printChar(byte c, int x, int y);
		void setXY(word x1, word y1, word x2, word y2);
		void clrXY();
		void rotateChar(byte c, int x, int y, int pos, int deg);
		void _set_direction_registers(byte mode);
		void _fast_fill_16(int ch, int cl, long pix);
		void _fast_fill_8(int ch, long pix);
		void _convert_float(char *buf, double num, int width, byte prec);
};

#endif

The cpp file is:

#include "Energia.h"


void setup();
void loop();


// UTFT_Bitmap (C)2012 Henning Karlsen
// web: http://www.henningkarlsen.com/electronics
//
// This program is a demo of the drawBitmap()-function.
//
// This demo was made to work on the 320x240 modules.
// Any other size displays may cause strange behaviour.
//
// This program requires the UTFT library.
//

#include <UTFT.h>

// Declare which fonts we will be using
extern uint8_t SmallFont[];

UTFT myGLCD(SSD1289_8, P1_4, P1_5, P1_6, P3_2);   // Remember to change the model parameter to suit your display module!

extern unsigned short int info[0x400];
extern unsigned short int icon[0x400];
extern unsigned short int tux[0x400];

void setup()
{
  Serial.begin(115200);
  Serial.println("hello world");
  myGLCD.InitLCD();
  Serial.println("initialised lcd");
  myGLCD.setFont(SmallFont);
  Serial.println("set font");
}

void loop()
{
//  myGLCD.fillScr(255, 255, 255);
  myGLCD.fillScr(0, 0, 0);
  Serial.println("filled screen");
  myGLCD.setColor(255, 255, 255);
  myGLCD.print(" *** A 10 by 7 grid of a 32x32 icon *** ", CENTER, 228);
  for (int x=0; x<10; x++)
    for (int y=0; y<7; y++)
      myGLCD.drawBitmap (x*32, y*32, 32, 32, info);
  Serial.println("drew bitmaps");

  delay(5000);
  
  myGLCD.fillScr(255, 255, 255);
  myGLCD.setColor(255, 255, 255);
  myGLCD.print("   Two different icons in scale 1 to 4  ", CENTER, 228);
  int x=0;
  for (int s=0; s<4; s++)
  {
    x+=(s*32);
    myGLCD.drawBitmap (x, 0, 32, 32, tux, s+1);
  }
  x=0;
  for (int s=4; s>0; s--)
  {
    myGLCD.drawBitmap (x, 224-(s*32), 32, 32, icon, s);
    x+=(s*32);
  }

  delay(5000);
}


**Attention** This is a public forum