Hi,
I am using FET Pro flash programming tool from Elprotronic to program the flash memory of EVM430-f6736 board.The IDE is IAR Embedded Workbench for MSP430 5.60. When I connected the msp430uif it asks for updating the firmware of the JTAG. I update this and when it reaches 100% updation, I closed that diologue box. For reading from flash what I will do further. Which file need to be written to the flash to download the program.