Hi all,
I'm working on my application that involves the On Board Programming of the MSP430F5151 device.
I'm developing the programming software using the SBW interface (2 wire JTAG), I followed the SLAU320m application note (pdf document and source code) and I used our hardware instead of the Replicator430Xv2 board as we had already done for other MSP devices.
I'm able to read the JTAG_ID, the DEVICE_ID (at address 0x01A04) and all other memory type (RAM, FLASH, registers) so I think that the ReadMem_430Xv2 , the ReadMemQuick_430Xv2 and the other LowLevel functions are working well but, unfortunately, I'm not able to write the registers (to disable the watchdog) or the RAM (to write the firmware for the erase or the programming) using the WriteMem_430Xv2 function.
Could someone help me to solve this problem?
Thanks in advance
Best regards
Alberto