Other Parts Discussed in Thread: LM35
Dear Sir/Madam,
I know basics of MSP430. I have plan to do the project with the help of MSP430 board.
Project Components are:
- Two stepper motor
- Capacitive touch Sensing -- (UP, DOWN, LEFT & RIGHT)
- Graphical LCD
- LM 35
These components or devices need to interface with MSP430 Board. Which MSP430 Board is suitable and which touch screen interface is suited for controlling motor UP, DOWN, LEFT & RIGHT rather than using buttons.
Please help how to connect Stepper Motor, Graphical LCD Interface & Capacitive Touch Sensor to the I/O Ports in MSP430 Board.
Thanks & Regards,
Deepan J