Other Parts Discussed in Thread: MSP430F5308
I'm having problems trying to use the I2C module USCI_B1 of an MSP430F5308 as master
My code is here:
#include <legacymsp430.h>
// P4.1 is data, P4.2 is clock
void initi2c(void)
{
UCB1CTL1|= UCSWRST; // reset
P4SEL |= BIT1|BIT2; // USCI_B1 I2C
P4REN |= BIT1|BIT2; // Enable pullups
// 7-bit address, single master, master mode, I2C mode, synchronous
UCB1CTL0 = UCMST|UCMODE_3|UCSYNC;
// smclk, transmitter, normal ack
UCB1CTL1 |= UCSSEL__SMCLK|UCTR;
UCB1BR0 = 0x7f; // 33 KHz scl ??
UCB1BR1 = 0;
// enable arbitration lost, not-acknowledge, start condition, transmit interrupts.
UCB1IE |= UCALIE|UCNACKIE|UCSTTIE|UCTXIE;
UCB1CTL1 &= ~UCSWRST; // release for operation
}
#define ERR_NOACK 1; // not acknowledge received
#define ERR_ARBT 2; // arbitration lost
int nbytes, done, error;
char *bufPtr;
interrupt (USCI_B1_VECTOR) i2cB1_Interrupt (void)
{
int iv = UCB1IV;
switch (iv)
{
case 2: // arbitration lost
error = ERR_ARBT;
done = 1;
break;
case 4: // not acknowledge
error = ERR_NOACK;
done = 1;
break;
case 6: // start condition received
UCB1TXBUF = *bufPtr++; // load first byte
nbytes--;
break;
case 0xc: // transmit buffer empty
if (nbytes)
{
UCB1TXBUF = *bufPtr++;
nbytes--;
}
else
{
UCB1CTL1 |= UCTXSTP; // generate stop
done = 1;
}
break;
default:
break;
}
}
int i2cWrite(char address, char *datap, int ndata)
{
nbytes = ndata;
bufPtr = datap;
done = 0;
error = 0;
UCB1CTL1|= UCSWRST; // reset
UCB1I2CSA = address;
UCB1CTL1 &= ~UCSWRST; // release for operation
UCB1CTL1 |= UCTXSTT; // generate START condition
while (!done)
;
return error;
}
The device I'm transmitting data to has address 0x46. However the address that is transmitted is 0x86 as shown by the following:
Another problem is that the not-acknowledge interrupt is not generated.
I'm sure I've done something wrong but I have no idea what. Your suggestions are appreciated.