Hi, all
After updating the FET, it is not possible to use the FET.
I've used the following procedure.
Software : FET-Pro430 Lite(Elprotoronic)
Hardware : MSP-FET430UIF
(1) Run FET-Pro430 Lite
(2) Click AUTO PROG
(3) Requested the Firmware update. I have run it
(4) Update had stopped at 97%.
(5) Later, FET Power lamp is not lighting, it is not possible to write MSP430 Flash memory.
Is there a way to solve this problem?
Best Regard,
FSSer