Hello,
im am running a MSP430F5659 at 19.2 MHz. The factory pre-programmed USB BSL does only suppport 4 MHz ,8MHz ,12MHz and 24 MHz.. I tried to use the USB BLS SLAA450 for the MSP430F552X and changed the device to MSP430F5569 as well as the 24MHz entry to 19.2 MHz. In addition i changed the XTAL2 sel port from SEL5 to SEL7. After uploading this bootloader to the device and calling the BSL by the adress 0x1000 i do not get a HID device recognized by my PC.
Do i have to make any other changes in source code to get the BSL running on my MSP5659 at 19.2 MHz?
Best regards
Stephan