I am prototyping using the MSP430 LaunchPad and the TI EPD Booster Pack from Pervasive Displays. I was successfully able to display images on the EDP. After this proof of concept, I am now ready to move onto the next phase of my project - Developing the actual circuit board. The problem is I don't know how or what components are needed.
My application is quite simple and is nearly exact to what the booster pack provided me:
- Connect microcontoller to a PC via micro USB
- Transfer a single, 4bit grayscale image from the PC to be displayed on 1.73" EPD
- Only one image will need to be stored and displayed.
Can anyone within TI or otherwise help me create this circuit so that I can integrate it into my full prototype?