Hi,
I encountered some problems in configuring the capture function 2 from P1.3 in timer A .
First. when a capture happens, Should I stop the timer by setting MCX=00, then read the value from the TACCR2?
Second. After I read the value, should I clear the TAR register to make sure the counter starts from 0?
Third, if the input frequency is low, will it cause timer A overflow?
Is there anyone could answer my questions. Thank you very much.