This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430-elf-gdb having issues on x86_64

$ msp430-elf-gdb 
Could not find platform independent libraries <prefix>
Could not find platform dependent libraries <exec_prefix>
Consider setting $PYTHONHOME to <prefix>[:<exec_prefix>]
'import site' failed; use -v for traceback
Traceback (most recent call last):
  File "<string>", line 1, in ?
ImportError: No module named os
GNU gdb (GDB) msp430-130423-90
Copyright (C) 2012 Free Software Foundation, Inc.
License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>
This is free software: you are free to change and redistribute it.
There is NO WARRANTY, to the extent permitted by law.  Type "show copying"
and "show warranty" for details.
This GDB was configured as "--host=i686-redhat-linux --target=msp430-elf".
For bug reporting instructions, please see:
<http://www.gnu.org/software/gdb/bugs/>.
(gdb) 

... is what I get when I try to start GDB on "Linux arch 3.14.4-1-ARCH #1 SMP PREEMPT Tue May 13 16:41:39 CEST 2014 x86_64 GNU/Linux"

Is there a bug tracker or similar for the Red Hat/TI gcc binutils stuff? I found a similar issue here: https://bugzilla.redhat.com/show_bug.cgi?id=488478


I might end up trying to get the source code to compile for x86_64 instead of using the pre-compiled 32 bit ELFs... which seems like it might fix the problem?

**Attention** This is a public forum