I have installed Code Composer both Under Linux Ubuntu 12.04 and through Virtual Box Lubuntu 12.04.
I can not connect to the MSP-EXP430G2 it says it can not find MSP-FET 430UIF.
06/07/14 11:50:11 PM ubuntu kernel [ 8258.560057] usb 1-2: new full-speed USB device number 3 using uhci_hcd
06/07/14 11:50:11 PM ubuntu mtp-probe checking bus 1, device 3: "/sys/devices/pci0000:00/0000:00:07.2/usb1/1-2"
06/07/14 11:50:21 PM ubuntu kernel [ 8268.829175] generic-usb 0003:0451:F432.0002: usb_submit_urb(ctrl) failed
06/07/14 11:50:21 PM ubuntu kernel [ 8268.829207] generic-usb 0003:0451:F432.0002: timeout initializing reports
06/07/14 11:50:21 PM ubuntu kernel [ 8268.831688] generic-usb 0003:0451:F432.0002: hiddev0,hidraw1: USB HID v1.01 Device [Texas Instruments Texas Instruments MSP-FET430UIF] on usb-0000:00:07.2-2/input1
06/07/14 11:50:21 PM ubuntu mtp-probe bus: 1, device: 3 was not an MTP device
06/07/14 11:50:21 PM ubuntu kernel [ 8269.109084] cdc_acm 1-2:1.0: This device cannot do calls on its own. It is not a modem.
06/07/14 11:50:21 PM ubuntu kernel [ 8269.109100] cdc_acm 1-2:1.0: No union descriptor, testing for castrated device
06/07/14 11:50:21 PM ubuntu kernel [ 8269.109291] cdc_acm 1-2:1.0: ttyACM0: USB ACM device
06/07/14 11:50:21 PM ubuntu kernel [ 8269.118578] usbcore: registered new interface driver cdc_acm
06/07/14 11:50:21 PM ubuntu kernel [ 8269.118602] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
06/07/14 11:50:21 PM ubuntu modem-manager[782] <info> (ttyACM0) opening serial port...
This is the information I see in the system log.
Please note that all connections in Energia work without a problem.
Not sure if the rules under /etc/udev/rules.d are created correctly.
It has been a real nightmare trying to get Code Composer Studio to work.
The only Version under Windows XP that works with the MSP-430 is 5.1
All the other versions have various installation problems.
Under Windows XP
Code Composer 6 hangs during the installation.
Code Composer 5.3 terminates with a Win32 exception during installation.
Code Composer 5.5 installs ok,but, when trying to connect to the target crashes and then exits the IDE.
Under Linux Ubuntu 12.04 and Lubuntu 12.04 cannot make connect to any target.
I have purchased a number of other LaunchPad Evaluations Kits
TM4C1294
EK-TM4C123GXL
I have spend over month trying to resolve these problems with no help from Texas Instruments.
This is my last try.
I will move on and purchase other chip sets for evaluation and never us Texas Instruments again.
Please note: I have called Texas Instruments on the phone and explained to them the problem and
they have been of no help. Not even and e-mail or phone call