Hi,
What is the maximum baud rate allowed in MSP430G2xxx series. Can it achieve a baud rate of 192Kbps ?
If yes:
1) what is the clock frequency I have to attach for a good communication?
2) How do I connect to PC with that speed. I do not see that speed mentioned in any terminal. Is there any other way?
Application: I am trying to interface MSP with a bluetooth module which can support upto 192Kbps via UART. This module pairs with the internal bluetooth of PC. Whenever it pairs, it creates a COM port from which the data can be received via terminal.
Waiting for the reply,
Thanks in advance