Other Parts Discussed in Thread: LM35, MSP430G2553
Hello,
I'm having problems interfacing the LM35 sensor with MSP4302553.
My code:
------------------------------------------------------------------------------------------------------------------------------------------------
#include <msp430.h>
#include <intrinsics.h>
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // STOP WATCHDOG
P1DIR = 0x1; // P1.0 OUTPUT
P1OUT = 0x0; // P1.0 OFF
ADC10CTL0 = SREF_1 | REFON | ADC10ON | ADC10SHT_3; // ADC SETTINGS
ADC10CTL1 = INCH_1 | ADC10SSEL_3 | CONSEQ_0;
ADC10AE0 = BIT1; // P1.1(A1) ANALOG INPUT
DCOCTL = 0; // CLOCK SETTINGS
BCSCTL1 = CALBC1_1MHZ;
DCOCTL = CALDCO_1MHZ;
TACTL = MC_1|ID_3|TASSEL_2|TACLR; // TIMER SETTINGS
TACCR0 = 62499;
TACCTL0 = CCIE;
__enable_interrupt();
for (;;)
{
__low_power_mode_0();
ADC10CTL0 |= (ENC | ADC10SC);
}
#pragma vector = TIMERA0_VECTOR
__interrupt void TA0_ISR(void){
__low_power_mode_off_on_exit();
}
}
--------------------------------------------------------------------------------------------------------------------------------------------
errors:
"../main.c", line 31: error #612: this kind of pragma may not be used here
"../main.c", line 32: error #68: expected a "}"
"../main.c", line 35: error #171: expected a declaration