This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi friends,
I want to run the motor using piezo electric crystals.
Here i need to get a power from piezoelectric crystals and stored it in battery. I use this power to run the motor.
I don't know which is possible or not. Because many documents says power from piezo is very low(Micro volts).
Please give suggestion for me...
I am eagerly waiting for ur replys...
Thanks in advance.
Regards,
Keerthi G
Power is not Volt. Power is Watt. A Piezo can reach high voltages (enough to make a spark in a gas lighter). However, the total energy per Piezo press is very low (only few µWs).
When you press a crystal, this results in a tiny charge moved on the surface of the Piezo. You can move this charge through a bridge rectifier into a capacitor. However, it will take lots of moves to collect as significant amount of energy in the capacitor. I doubt you’ll be able to continuously operate a motor with it. But of course this can be used to (re)charge a battery for a sensor module that runs on very low power.
Nevertheless, this topic is in the wrong forum, as this is the MSP430 MCU forum. J
**Attention** This is a public forum