Dear All
I am using MSP430F6438 internal DAC, and have configured the Control registers for 3x output gain. The reference voltage is derived from REF module 2.5 V.
I expect the maximum output from the DAC when i write 0xFFF in Data registers as 7.5 V.
But what ever may be the settings in DAC12IR and DAC12OG. The range of output from the DAC is always 0-Vref.
Somehow the multiplier seems to be not working.