Other Parts Discussed in Thread: MSP430F2370
Hi,
My connection is below:
MSP430G2 launchpad Target board connections (MSP430F2370)
Vcc Vcc
GND Gnd
P1.6 P1.1 BSL Tx
P1.7 P2.2 BSL Rx
P1.4 RST
P1.0 TCK
The above connections are done, able to invoke BSL and load the .txt file from the script.
As per the requirement should be able to load the firmware over the actual UART pins i.e P3.4(UCA0TXD) and P3.5(UCA0RXD) instead of BSL Tx and Rx, as P3.4 and P3.5 is connected to PC for firmware upgrade over RS232. So how to make it working?? or it should be done always over BSL Tx and Rx??
Thanks.
Best Regards,
Santosh.