Other Parts Discussed in Thread: MSP430F5510, CCSTUDIO
I'm trying to calculate the maximum current consumption that the MPS430F5510 may consume during flash programming. I intend to use the on-board supply (as opposed to the programmer supply) to power the MSP430 during programming, but want to make sure my supply can source sufficient current.
From the 5510 datasheet, I see that an erase operation can draw a maximum of 6.5 mA, which I would add to the active mode supply current. The question is what PMMCORE and frequency can I expect the MSP430 to be in during programming? Are there any other functions that I would need to add in?