Hi,
I am using MSP-TS430PZ100C Evaluation board for MSP430F6438 chip and MSP-FET debugger with IAR IDE, version "6.10.1".
After I create a .hex output file and try to download the file, I get the following error:
Wed Jul 16, 2014 19:47:00: Firmware version 30400020
Wed Jul 16, 2014 19:47:00: Interface dll version 3.4.0.20
Wed Jul 16, 2014 19:47:05: Device : MSP430F6438
Wed Jul 16, 2014 19:47:05: External voltage : 0.0 V
Wed Jul 16, 2014 19:47:05: VCC voltage : 3.3 V
Wed Jul 16, 2014 19:47:06: Loaded debugee: <Path to the hex file>
Wed Jul 16, 2014 19:47:06: Target reset
Wed Jul 16, 2014 19:47:06: Invalid parameter(s) : (SetEEMSequencer)
I use the following procedure to generate the hex file:
Options -> Linker -> Output
Select "Other" radio button and choose intel extended as the output format
Check override default and give .hex extension to the output file name.
In addition to the "Download file" option, if I select "Download active application" or "Erase memory" option I get the same error.
Same happens with ".d43" file download.
Please help to resolve this issue.