Hi,
According to the table here http://www.ti.com/tool/energytrace (row 6, column 2) to enable EnergyTrace on any MSP430 device you need MSP-FET. Shouldn't it be MSP-FET or MSP-EXPFR5969?
What is the sampling rate using MSP-FET and using MSP-EXPFR5969? (I have a number of old MSP-FETs and considering to get a new one.)
Can I setup CCS and EnergyTrace for continuous monitoring of current or only snapshot?
Can I use EnergyTrace to monitor external load? For example if I connect a potentiometer as a load in parallel with MSP430 MCU running in low power mode
Thanks
Jan.