Im trying to communicate with my EXP430F5529 LP over backchannel UART (UCA1). The transmission from MSP to PC is working fine - it gets displayed in the Putty terminal. However, when I write a character in Putty, the UCRXIFG gets never set (when I halt the program with debugger, I can see it is stuck inside USCI_A_UART_receiveData polling for the UCRXIFG flag) - see the source code below.
SMCLK set to 1MHz, baudrate 9600
Im using MSPWare 1.90 Driverlib. Here is my source code:
void initClocks(uint32_t mclkFreq)
{
// Assign the REFO as the FLL reference clock
UCS_clockSignalInit(
UCS_FLLREF,
UCS_REFOCLK_SELECT,
UCS_CLOCK_DIVIDER_1);
// Assign the REFO as the source for ACLK
UCS_clockSignalInit(
UCS_ACLK,
UCS_REFOCLK_SELECT,
UCS_CLOCK_DIVIDER_1);
UCS_initFLLSettle(
mclkFreq/1000,
mclkFreq/32768);
//use REFO for FLL and ACLK
UCSCTL3 = (UCSCTL3 & ~(SELREF_7)) | (SELREF__REFOCLK);
UCSCTL4 = (UCSCTL4 & ~(SELA_7)) | (SELA__REFOCLK);
}
void transmitBytes(uint8_t* bytes,uint8_t size)
{
for (uint8_t i = 0;i < size;++i)
{
USCI_A_UART_transmitData(USCI_A1_BASE,bytes[i]);
}
}
int main( void )
{
// Stop watchdog timer to prevent time out reset
WDTCTL = WDTPW + WDTHOLD;
// Set clock to 1MHz
initClocks(1000000);
// Set LED and blink
setupLEDs();
blinkLED1(2);
// Setup pins
GPIO_setAsPeripheralModuleFunctionInputPin(
GPIO_PORT_P4,
GPIO_PIN4 + GPIO_PIN5
);
// Initialize UART (baudrate 9600)
USCI_A_UART_initAdvance(USCI_A1_BASE,USCI_A_UART_CLOCKSOURCE_SMCLK,
104,0,1, USCI_A_UART_NO_PARITY,
USCI_A_UART_LSB_FIRST,USCI_A_UART_ONE_STOP_BIT, USCI_A_UART_MODE,
USCI_A_UART_LOW_FREQUENCY_BAUDRATE_GENERATION);
USCI_A_UART_enable(USCI_A1_BASE);
uint8_t hello[6] = {'M','S','P','4','3','0'};
transmitBytes(hello,6);
while (1)
{
// Wait for incoming byte
uint8_t recv = USCI_A_UART_receiveData(USCI_A1_BASE);
blinkLED2(2); // Blink led when data is received
// Perform the received command
if (recv == 'A')
{
blinkLED1(5);
}
else if (recv == 'B')
{
blinkLED2(5);
}
else if (recv == 'C')
{
uint8_t hello[6] = {'H','E','L','L','O','!'};
transmitBytes(hello,6);
}
else if (recv == 'Q')
{
break;
}
}
// Close UART peripheral
USCI_A_UART_disable(USCI_A1_BASE);
return 0;
}
Im running Windows 7 with IAR. Of course, I set 9600 baudrate, stop bits, no parity, etc. in putty accordingly.
Also the RXD and TXD jumpers on my LaunchPad are in place.
Thanks for any hints!