Can I plug in a 3.3V source on the Vcc pin *and* plug in the USB? I know the launchpad can be powered via usb, so If I plug in both does something intelligent go on that prevents the voltages from fighting each other? I ask because I need to download data over USB but the launchpad will be in the field doing data logging where the USB is not connected, so we need the external power source as well.
Since this will be a project used by students, I suspect that some of them will plug in the USB without first unplugging the external source, so hopefully it's not a problem...
Mike