I am using the MSP430F5510 and I need to create a custom bootloader to handle OTA updates, the radio stack that I will be using is the SimpliciTI and so the code footprint will be greater than that of the 2k available for the BSL so I will need to create my own bootloader that resides in the main flash and is called from the BSL. Could someone please provide a document that can get me started on a custom bootloader for the MSP430F5510, one that uses UART would be helpful just so I can get the skeleton and build on it.
Thanks,
Callum